REC.TRIGTYPE

Description

REC.TRIGTYPE sets the type of trigger.

Input values are as follows:

Value

Description

0

Recording starts immediately

1

Next command: Recording starts on the next command executed through the TCP/IP. The trigger location in the buffer is set according to REC.TRIGPOS .

2

Source signal: Recording starts per the values of REC.TRIGPARAM, REC.TRIGVAL , REC.TRIGSLOPE , and REC.TRIGPOS .

3

Boolean: Recording starts when the value of REC.TRIGPARAM is 0 for REC.TRIGSLOPE = 0 or 1 for REC.TRIGSLOPE = 1

4 Exact: Recording starts when the value of REC.TRIGPARAM is exactly the value specified REC.TRIGVAL and change happened with REG.TRIGSLOPE slope.
5 Bitmask: Recording starts when the value of REC.TRIGPARAM masked by REC.TRIGMASK matches REC.TRIGVAL with slope REC.TRIGSLOPE.

Example

Code

If REC.TRIGPARAM is DIN.STATES and REC.TRIGMASK = 0x3, then the triggering happens only when both DIN1 and DIN2 are high.

-->REC.TRIGTYPE 5

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 5

Default Value

0

Data Type

Integer

See Also

REC.TRIG , REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE REC.TRIGPOS

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REC.TRIGTYPE

2310

906

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REC.TRIGTYPE

2310

Unsigned8

Read/Write

-